Check box example

Check box example

Use this object to set and view a Boolean value at runtime.
Selected check box
The associated variable value is True.
Cleared check box
The associated variable value is False.
Check box example
animated graphic showing selecting and clearing a check box

Use case

Enable or disable functions or features within a
FactoryTalk Optix Application
. For example, toggle a graph that visualizes data.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal