Object editor

Object editor

The editor for an object is the main design canvas of
FactoryTalk Optix Studio
. The path to the object appears in the upper left corner and contains the node and object type.
The Object editor toolbar contains buttons that apply to the selected object. The buttons displayed depend on the object selected in the editor. In general, the buttons position the object on the canvas of the editor. For example, the buttons change the order of stacked objects and position the object on the top, bottom, or either side of the canvas. Buttons are disabled in the toolbar if an object is not selected on the editor canvas.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.