- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Output pane
The
Output
pane contains columns of message information and buttons to perform tasks on the Output
pane. By default, the Output
pane displays errors of minimum and maximum severity and information messages. Enable Advanced mode
to display information in the Output
pane.Select the arrow in the column heading to display the messages in ascending or descending order. Message columns support filtering.
Column | Description |
---|---|
Message security level | ![]() ![]() ![]() |
Code | Message ID code. This code is for predefined FactoryTalk Optix Studio messages only. |
Timestamp | The time the message was logged. |
Category | The category of the FactoryTalk Optix Platform message or module that generated the message. |
Object | Any element referenced by the message. |
Message | The content of the message. |
Item | Description |
---|---|
![]() | Display or hide error messages of maximum severity. |
![]() | Display or hide error messages of minimum severity. |
![]() | Display or hide information messages. |
![]() | Display or hide first level verbose messages for troubleshooting. |
![]() | Display or hide second level verbose message for troubleshooting. |
![]() | Open the output logs folder. For more information, see System log. |
![]() | Delete all messages from the Output pane, regardless of the selected display. Messages are not deleted from log files. |
Provide Feedback