Properties pane

Properties pane

Use the
Properties
pa
ne to display variables for the selected object. Property values change the appearance and display of that object at runtime. The
Properties
pane also displays
Events
for the selected object.
An event is something that occurs to trigger an action called a method. Events initiate on the HMI device in runtime.
Properties pane buttons
Item
Description
Function
Group by category
Organize the properties by category.
Sort alphabetically
Sort the properties in alphabetical order.
Add new
Add a property to the node. Add a display name, variable, alias, or audit signature.
In the
Events
category of the
Properties
pane, this button adds a new event from the
Events
header or a new method for the selected event.
Delete
Remove an added property from the
Properties
pane or reset the value of a default property.
In the
Events
category of the
Properties
pane, this button deletes the selected method. Removing all methods from an added event deletes the event.
Open with editor
Open the editor for the selected object. This button is valid for only certain object types.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.