- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Graphic objects library
FactoryTalk Optix Studio
has a library of default graphic objects for creating user interfaces for your FactoryTalk Optix Applications
. These objects are available in the Types
inside the User interface
folder. Graphic objects include:
- Basic controls. Objects such as labels, text boxes, buttons, and analog indicators.
- Containers. Objects that create the basic graphical structure of the application. Containers can contain other objects such as other containers, panels, and sections that have automatic content alignment.
- Contents. Objects such as the web browser, video, and PDF viewer, that display application contents.
- Data controls. Objects that display project node or database data and allow you to select that data. Data controls include data grids, combo boxes, and trend graphs.
- Drawings. Objects that add shapes and images to theFactoryTalk Optix Application.
Provide Feedback