Data controls objects

Data controls objects

Data controls objects include:
Object
Description
Combo box
Drop-down to select elements from project nodes or one or more databases.
List box
List to select element within other elements or either project nodes or databases.
Data grid
Table that presents data from project nodes or databases.
Trend
Trend that presents values from one or more variables that are logged or read in real time.
XY chart
Chart that displays the value of two-dimensional variables in a graph.
Pie chart
Chart that displays model or database data in the form of a pie chart.
Histogram chart
Chart that displays model or database data in the form of a bar chart.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.