- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Push Agent configuration for Azure IoT Hub
An example of Push Agent configuration for sending and receiving data with Azure IoT Hub broker.
Property | Value |
---|---|
ClientId | MyDevice01 |
BrokerIPAddress | contoso.azure-devices.net |
BrokerPort | 8883 |
BrokerTopic | devices/MyDevice01/messages/event/ |
QoS | 1
IMPORTANT:
Azure Iot Hub does not support level 2 QoS. If you use the level 2 QoS, Azure Iot Hub closes the connection every time a message is sent.
|
UseSSL | True |
CACert | |
ClientCert | |
ClientCertPassword | |
Username | contoso.azure-devices.net/MyDevice01/?api-version=2018-06-30 |
Password | SharedAccessSignature sig= signature-string &se=expiry &sr=URL-encoded-resourceURI |
Provide Feedback