Import an OPC UA NodeSet
Import an OPC UA NodeSet in either online or offline mode.
Prerequisites
- If you import the NodeSet in the offline mode, obtain the NodeSetXMLfile.
- To import an OPC UA NodeSet
- InProject view, right-click the OPC UA client object and select .OPCUATagImporterappears under the OPC UA client object.
- Next toOPCUATagImporter, select
.
- Configure the NodeSet import:
- If you import the NodeSet in the online mode, set the toggle toOnline.
- If you import tags in the offline mode:
- Set the toggle toOffline.
- InFile path, provide a path to theXMLfile with the NodeSet.
- Select the items to import and then selectApply.
The imported objects appear under the OPC UA client.
Provide Feedback