Import nodes at design time

Import nodes at design time

Import nodes by using the OPC UA tag Importer object.
  1. In
    Project view
    , right-click an OPC UA client object and select
    New
    OPC UA tag importer
    .
  2. Double-click the
    OPCUATagImporter
    object.
    • FactoryTalk Optix Studio
      connects to the server.
    • In the central pane, the editor shows the list of nodes that can be imported.
    • An
      Objects
      node is created inside the
      OPCUAClient
      object.
  3. In the editor, select the nodes and select
    Synchronize
    .
The project nodes corresponding to the selected nodes are added to the
Objects
node.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal