Develop a temperature change alarm
Develop an alarm that signals when temperature exceeds a set value.
Application example

NOTE:
Download a sample project:
TemperatureChangeAlarm.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example

In
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
FactoryTalk Optix Studio
, select Run
Provide Feedback