Create a temperature alarm

Create a temperature alarm

Create an alarm that warns you when a set temperature value is exceeded.
  1. Create an input variable:
    1. In
      Project view
      , right-click
      Model
      and select
      New
      Variable
      .
    2. Hover-over the variable, select
      Edit
      , and enter
      TemperatureAlarmVariable
      :
  2. Create the alarm:
    1. In
      Project view
      , right-click
      Alarms
      and select
      New
      Exclusive level alarm
      .
    2. Hover-over the alarm, select
      Edit
      , and enter
      TemperatureAlarm
      .
  3. Configure the Alarm:
    1. In
      Properties
      , create a dynamic link between the
      Input variable
      property and
      ProjectName
      Model
      TemperatureAlarmVariable
      .
      For more information about dynamic links, see Create dynamic links.
    2. Set
      High limit
      to
      75
      .
    3. Set
      Auto confirm
      to
      True
      .
    4. Set
      Message
      to
      Temperature exceeds a safe level!
      .
    5. Set
      Severity
      to
      3
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal