Develop a motor management dashboard
The UI contains a list of motors and gauges that display speed and acceleration values.
Application example

NOTE:
Download a sample project:
MotorManagementDashboard.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.

In
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
FactoryTalk Optix Studio
, select Run
Provide Feedback