Create a list of motors

Create a list box populated with motor objects.
  1. In
    Project view
    , right-click
    MainWindow (type)
    and select
    New
    Data controls
    List box
    .
  2. Hover-over the list box, select
    Edit
    , and enter
    MotorListBox
    .
  3. In
    Properties
    , create a dynamic link between
    Model
    and
    ProjectName
    Model
    MotorObjects
    For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.