Develop a gauge with a localized engineering unit

Develop a gauge with a localized engineering unit

Create a linear gauge that displays the current temperature in a format adjusted to the logged in user.
Application example - Celsius degrees (it-IT)
Application example - Fahrenheit degrees (en-US)
NOTE:
Download a sample project:
LocalizedEngineeringUnitGauge.zip
Prerequisites
  1. To develop the project
  2. Arrange the interface elements.
  3. Save the project.
Application design example
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal