Debug runtime NetLogic remotely
With Visual Studio, you can remotely debug a runtime NetLogic on Windows systems.
TIP:
Remote debugging is not possible on HMIs for security reasons. For more information about remote debugging, see Remote debugging - Visual Studio (Windows) | Microsoft Learn.
To debug NetLogic locally, see Debug NetLogic.
- On the development machine, download Visual Studio and set as the default code editor. See Set the default code editor.
- Verify that the client machine and the development machine are connected to the same network.
- Configure the remote Windows machine as a target inFactoryTalk Optix Studio. See Add a deployment target device.
Provide Feedback