Add a deployment target device

Add a device  to run
FTOptixApplications
.
  1. From the
    FactoryTalk Optix Studio
    toolbar, next to
    Run
    , select the down arrow and select
    Configure target device
    .
  2. In the
    Deployment target device configuration
    window, select
    Add
    Add new target
    .
  3. Fill in the fields.
  4. Select
    Close
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.