- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Deploy a FactoryTalk Optix Application from a USB drive
To deploy a
FactoryTalk Optix Application
from a USB drive, move the file to the client device and run the file.Prerequisites
- Move the file from the USB drive to the client device.
- RunFactoryTalk Optix Applicationon the client system:
- OnWindows®client devices, double-clickFTOptixRuntime.exe.
- On Linux client devices, in the terminal, navigate to theFTOptixRuntimefile folder and enter./FTOptixRuntime.
Provide Feedback