Export a FactoryTalk Optix Application to a USB drive
Export a
FactoryTalk Optix Application
to a USB drive to deploy the FactoryTalk Optix Application
to client devices that are not accessible in the network.- InFactoryTalk Optix Studio, select the arrow next toto open the drop-down menu.Save
- Selectto open theExport to USBdialog.
- InExport to USB, complete:
- Platform. Select the operating system of the client device.
- USB drive. Select the USB drive to which to export the application.
- Username. Specify the administrator account of the client device.
- Password. Specify the password of the administrator account.
- Clear application files. Select to overwrite an existingFactoryTalk Optix Applicationon the client device and delete the runtime files associated with that application. Clear if the application is installing while the existing application is still running.
- SelectExport.
Provide Feedback