Configure a transitioned event

Configure a transitioned event

Trigger methods if the value of a variable or object property meets a specific condition.
  1. In
    Project view
    , select an object or a variable.
  2. In
    Properties
    , right-click a variable or a property and select
    New
    Transitioned event
    .
    TIP: If needed, select
    Add
    to add a variable.
  3. In
    Events
    , from
    Transition
    select:
    • Equal to
    • Not equal to
    • Greater than
    • Greater than or equal to
    • Less than
    • Less than or equal to
  4. Set the
    Value
    property.
    TIP: You can enter the threshold value or add a dynamic link to the threshold value. For more information about dynamic links, see Create dynamic links.
  5. Next to
    VariableTransitioned
    , select
    Add
    .
  6. Select a method:
    • For global methods, expand
      Commands
      .
    • For local methods, expand the nodes that expose methods (for example, a
      DataGrid
      node exposes a
      Refresh
      method), or expand the node related to a specific NetLogic.
  7. (optional) If the method requires arguments, expand the method and set arguments.
  8. (optional) Select more methods by repeating 5 through 7.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal