Drawing tools
Use drawing tools to create custom graphic objects to appear at runtime.
Use the drawing tools to draw free-form and one-dimensional objects including:
- Rectangles and squares
- Ovals and circles
- Lines
- Polylines and polygons
By default, each drawing object has a
MouseDown
event and MouseUp
event to which you can add methods that the event performs.To prevent a drawing from snapping to the grid as you draw, in
, clear
Snap to grid
. Provide Feedback