Graphic and layout objects

Graphic and layout objects

Use graphic and layout objects to create a
FactoryTalk Optix Application
user interface.
To create the user interface, design:
  • Structure and hierarchy of graphic objects
  • Position of graphic objects
  • Navigation mechanisms
TIP: The user interface design is independent of the device and the presentation technology used to display the application at runtime.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal