Graphic objects library

Graphic objects library

FactoryTalk Optix Studio
has a library of default graphic objects for creating user interfaces for your
FactoryTalk Optix Applications
. These objects are available in the
Types
inside the
User interface
folder.
Graphic objects include:
  • Basic controls
    . Objects such as labels, text boxes, buttons, and analog indicators.
  • Containers
    . Objects that create the basic graphical structure of the application. Containers can contain other objects such as other containers, panels, and sections that have automatic content alignment.
  • Contents
    . Objects such as the web browser, video, and PDF viewer, which display application contents.
  • Data controls
    . Objects that display project node or database data and allow you to select that data. Data controls include data grids, combo boxes, and trend graphs.
  • Drawings
    . Objects that add shapes and images to the
    FactoryTalk Optix Application
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.