Base control objects
Base control objects include:
Object | Description |
---|---|
Label | Displays text that describes an item. |
Text box | Inserts and displays text at runtime. |
Spin box | Increases or decreases a numerical value using buttons or keys. |
Editable label | Displays and editable description of an item. |
LED | Displays a Boolean value in the form of an on LED or an off LED. |
Button | Generates events to perform methods. |
Switch | Sets and displays a Boolean value. |
Checkbox | Sets and displays a Boolean value using select and clear. |
Option button | Selects a mutually exclusive option in a group. |
Linear gauge | Sets or displays an integer value within a range of possible values. |
Circular gauge | Sets or displays an integer value within a range of possible values. |
Date and time | Displays date and time data. |
Duration | Displays the duration of a variable. |
Provide Feedback