- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Container objects
Container objects include:
Object | Description |
---|---|
Panel | Simple container of graphic objects that can be a selectable area. |
Horizontal layout | Panel that automatically arranges graphic objects horizontally next to each other. |
Vertical layout | Panel that automatically arranges graphic objects vertically next to each other. |
Scale layout | Container that automatically scales its children graphic objects when the container aspect ratio changes. |
Panel loader | Container that uses logic to display different alternative panels at runtime. |
Navigation panel | Panel that contains other panels and automatically organizes panels into tabs that you can navigate. |
Dropdown button | Button that, when selected, opens and closes a pop-up window. |
Scroll view | Panel that can scroll to display content larger than the panel size. |
Accordion | Container that contains expandable content blocks. |
Window | Root graphic container. In a Presentation Engine, you can set Window to specify the initial user interface at runtime.
TIP:
The
X , Y , and Always on Top properties apply only to the Native Presentation Engine. |
Provide Feedback