Add limits to a variable
Add minimum and maximum limits to numeric variables. Limits impose certain behaviors when the value is outside of the limits.
- InProject view, select the variable.
- InProperties, right-click the numerical variable and select .
- UnderEURange, complete:
- Low limit. Enter the low limit for the value of the variable.
- High limit. Enter the upper limit for the value of the variable.
- Constrain. Set to true to constrain the values for the variable for the low and high limits.
Provide Feedback