Variables

Variables

A variable is an attribute of an object. Assign a value to a variable to display the value at runtime.
View variables in
FactoryTalk Optix Studio
from either:
  • Project view
    . Navigate to the folder containing the variables. The
    UI
    folder cannot contain variables.
  • Properties
    . Select an object, type, or variable in
    Project view
    or select and object in the editor. The variables or properties for the selected item appear in
    Properties
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.