Change the unit of measure for a variable
Change the unit of measure for a variable that displays at runtime.
- InProject view, select the variable.
- InProperties, select the unit of measurement in the value of the variable.
- In theEUInformation Editor, select the unit of measure and chooseSelect.
The new unit of measure appears in the value for the variable.
Provide Feedback