Remove a unit of measure from a variable
Remove the unit of measure for a variable to no longer have the value for that variable appear in that unit of measure.
- InProject view, select the variable.
- InProperties, in the value for the variable, select the unit of measure.
- In theEUInformation Editor, select the unit of measure and selectDelete.
- SelectOK.
The unit of measure is removed from the variable.
Provide Feedback