Configure network interface settings

Configure network interface settings

Configure the network interface to create the network interface and name the interface type.
  1. In
    Project view
    , expand the object and select the
    System
    object.
  2. In
    Properties
    , next to
    Network interfaces
    , select
    Add
    NetworkInterface
    .
    NetworkInterface
    #
    appears in
    Properties
    with settings to display and edit at runtime.
  3. In
    Interface name
    , enter an interface type exactly as it appears in
    FactoryTalk Optix System Manager
    .
    • LAN
    • WAN
    • Wi-Fi
  4. If necessary, configure the network properties:
    • DHCP activated
      . Enable or disable automatic IP address assignment in DHCP mode.
    • IP address
      . Primary IP address.
    • Mask
      . Subnetwork mask.
    • DNS 1
      . DNS1 IP address. For WAN and Wi-Fi interfaces only.
    • DNS 2
      . DNS2 IP address. For WAN and Wi-Fi interfaces only.
    • Gateway
      . Default gateway IP address.
    • Additional IP addresses
      . Additional IP addresses of the interface. For Lan interface only.
  5. Repeat 2 through 4 for each additional network interface.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal