System object

System object

The
System
object allows you to access system settings that provide information such as example date and time and the IP addresses of network interfaces.
Add the
System
object to a project when you want the user to be able to view and reconfigure these settings and restart the system at runtime.
TIP: The settings that are accessible through the
System
object are available through the
FactoryTalk Optix System Manager
. All object functions are available on
FactoryTalk Optix Panels
. Only the restart function is available in Windows.
If
FactoryTalk Optix System Manager
does not allow you to perform an operation through the
System
, an error message is thrown. If the configuration is incorrect, the last correct values are set in the
System
object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.