- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Configure the Network Configurator widget
Configure the
Network Configurator
widget to display and edit the Settings for WAN, LAN, and Wi-Fi network interfaces.Prerequisites
- To configure the Network Configurator widget
- Select.Template Libraries
- InLibraries, selectWidgets.
- UnderComponents, dragNetwork ConfiguratorintoProject view.
- InLibraries, selectClose.
- InProject view, expandNetworkConfiguratorDialog(type)to displayPropertiesfor the type.
- Drag theSystemobject to#SystemNodeinProperties.The system settings are associated with the widget.
- At runtime, perform the desired edits, and then selectApply.
Provide Feedback