Create the System object
The System object allows users to view and configure certain system settings, such as those that provide the date, time, time, and IP addresses of network interfaces and allows the user to restart the system at runtime.
Create one
System
object per project. - InProject view, right-clickModeland then select .System1appears inProject view.
Provide Feedback