Configure the Date and time configurator widget

Configure the Date and time configurator widget

Configure the
Date and time configurator
widget to display and edit the system date, time, and time zone manually or through a remote NTP server.
  1. To configure the Date and time configurator widget
  2. Select
    Template Libraries
    .
  3. In
    Libraries
    , select
    Widgets
    .
  4. Under
    Components
    , drag
    Date and time configurator
    into the
    UI
    folder in
    Project view
    .
  5. In
    Libraries
    , select
    Close
    .
  6. In
    Project view
    , in the
    UI
    folder, select the
    DateAndTimeConfigurator (type)
    to display
    Properties
    for the type.
  7. Drag the
    System
    #
    object to
    SystemNode
    in
    Properties
    .
    The system settings are associated with the widget.
  8. At runtime, perform the desired edits, then select
    Apply
    .
  9. Close the application and restart the system for the date and time changes to take effect. See Create a button to restart the system.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.