Trends

Use a
Trend
object to display how values change over time. You can display data from a database or sample it in real time.
Trend example
a trend graph showing the change in two variables over time

Runtime

You can interact with the Trend graph at runtime to see additional information.
TIP: Some actions require the
Interactive
property value to be
True
. For more information about the properties of a
Trend
object, see Trend and Trend pen.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.