Create an analog variable
Create an analog variable that indicates temperature.
- InProject view, right-clickModeland select
- Configure the variable:
- InProperties, set theAnalogVariable1 (Float)property value to50.
- Next to the property value, select<None>and selectTemperature: degree Fahrenheit
- UnderEURange, setLow limitto-10.
- Set theHigh limitto60.
- Set theConstraintoTrue.
Provide Feedback