Develop a gauge with a localized engineering unit

Develop a gauge with a localized engineering unit

Create a linear gauge that displays the current temperature in a format adjusted to the logged in user.
Application example - Celsius degrees (it-IT)
Application example - Fahrenheit degrees (en-US)
NOTE:
Download a sample project:
LocalizedEngineeringUnitGauge.zip
Prerequisites
  1. To develop the project
  2. Arrange the interface elements.
  3. Save the project.
Application design example
elect
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal