Add users
Add users with different locales.
Prerequisites
Add the it-IT locale. See Add a locale language to a localization dictionary.
- To add users
- InProject viewpane, expandSecurity.
- Create two users by right-clickingUsersand selecting .
- Rename the users by hovering-over each user, selecting, and entering:
- Alice
- Jeremy
- InProject view, selectAlice.
- InProperties, set theLocaleIdsproperty value toit-IT.
Provide Feedback