Develop a recipes management dashboard
Create a dashboard to add, remove, and modify recipes based on a recipe schema.
The dashboard interface also incorporates additional gauges for displaying and controlling the maximum RPM and minimum throttle values of the motor.
NOTE:
Download a sample project:
RecipesManagementDashboard.zipPrerequisites
- To develop the project
- Create and configure a recipe schema. See Configure a recipe schema or Configure a recipe schema manually.While creating the recipe:
- Create a dynamic link between theTarget nodeproperty and .For more information about dynamic links, see Create dynamic links.
- Select theand parameters.TIP: These parameters will be configurable at runtime.
- Add and configure a default recipes editor widget. See Configure a recipes editor widget.
- Arrange the interface elements.
- Save the project.
elect to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback