- Getting started
- Using the software
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Recipes editor
The recipes editor widget contains the graphical objects and NetLogic scripts required to display and manage the recipes at runtime.
Use the recipes editor widget to:
- Display ingredients and values of a stored recipe during editing or loading the controller
- Create, edit, or delete a recipe
- Store a recipe in the database
- Load a recipe from theFactoryTalk Optix Applicationto the controller
- Load a recipe from the controller to theFactoryTalk Optix Application
Recipes editor interface
Recipes editor example

Item | Name | Description |
---|---|---|
![]() | Recipe name | Assign a name to a new recipe or select an existing recipe. |
![]() | Recipe control buttons |
|
![]() | Ingredients list | Recipe schema ingredients. |
![]() | Ingredient values editor | Editable values of the recipe ingredients. |
![]() | Applied ingredient values | Values of the ingredients on the controller. |
Provide Feedback