Design a recipes management interface
You can use the default recipes editor to add new recipes, delete existing recipes, or apply recipes on the controller.
TIP:
You can develop your own recipes management solution. For more information, see Custom recipes management interface.
Prerequisites
Configure a database to store recipes at runtime. See Create an embedded database or Create an ODBC database.
- To design a recipes management interface
Provide Feedback