Develop automatically generated UI
Develop a UI populated automatically with graphical elements based on the properties of objects in the Model folder.
NOTE:
Download a sample project:
UIGeneratedFromModel.zipExample application
![](/content/dam/dita/en/factorytalk-optix/1-10/_images/UIGeneratedFromModel1.png/_jcr_content/renditions/original)
![](/content/dam/dita/en/factorytalk-optix/1-10/_images/UIGeneratedFromModel2.png)
Prerequisites
- Download, extract, and copy the images into thefolder.ProjectName/ProjectFiles
- To develop the project
- Arrange the interface elements.
- Save the project.
![](/content/dam/dita/en/factorytalk-optix/1-10/_images/UIGeneratedFromModelDesign.png/_jcr_content/renditions/original)
elect
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback