Implement the UIPopulator NetLogic
Point the NetLogic to the graphic objects.
- InProject view, selectUIPopulator.
- InProperties, at the top, selectand selectVariable.
- Hover-over the variable, select, and enterModelObject.
- Next toModelObject, selectInt32and selectNodeId.TIP: If you do not see the required option, select theShow allcheckbox.
- Create a dynamic link betweenModelObjectand .
Provide Feedback