XY Chart
Use this object to display the value of two-dimensional variables in a Cartesian chart.
XY chart example

Use case
Graphically represent or set machine processes, for example the cutting profile or the work area within which a machine can operate.
TIP:
You can disable the display of a pen by setting its
Enabled
property to False
.Provide Feedback