Add an array line pen
Add an array line pen to visualize the distance between the values of a two-dimensional variable.
- InProject view, select or create a two-dimensional variable of theNumberdata type.For more information, see Variables.For example, create a variable of theNumber[2,2]data type.
- elect or create anXYChartobject.
- InProperties, next toPens, selectand selectArray line pen.
- Create a dynamic link betweenPoint arrayand the two-dimensional variable.For more information about dynamic links, see Create dynamic links.
- (optional) Make the array line pen editable at runtime:
- Set theEditableproperty toTrue.
- InPoint array, selectand selectChange Dynamic LinkAdvanced.
- In theComplex Dynamic Link Editor, set the link direction to
.
Provide Feedback