Communication driver

Communication drivers

Use communication drivers to establish connections with controllers and import tags. Use controller tags to design application logic.

Communication driver objects

Each communication driver consists of the following objects hierarchy:
  • Communication driver
    . Represents a communication protocol.
    • Communication station
      . Represents a physical controller.
      Communication driver
      can contain multiple
      Communication station
      objects.
      • Tags
        . Contains tags imported from the controller.
        Each imported tag creates a corresponding Tag project variable. The values and data types of Tag variables remain synchronized with the values of the tags on the controller at runtime in read mode and in write mode.
        TIP: When the controller Tag Data Type does not match an OPC UA standard Data Type, the most relevant OPC UA Data Type is set for the variable.
      • Types
        . Contains types imported from the controller.
      • TagImporter
        . Depending on the
        Communication driver
        , allows you to import tags from controllers in the online or offline mode.
        Use the offline mode to import a file with tags exported from the controller. Use the online mode to establish a connection with the controller in the network and import tags from the controller.
You can communicate with controllers that support custom protocols through the serial interface by using the
Serial port
communication driver. For advanced implementations, you can use dedicated C# APIs. See C# APIs reference.

Runtime communication

Keep the values and data types of the imported tags synchronized with the controller. Tags synchronize at regular intervals based on the
Dynamic variables polling time
value of Presentation Engines.
To optimize read/write operations,
FactoryTalk Optix Studio
synchronizes the tags displayed or written through the active graphical objects. To save bandwidth, controller tag values update at runtime only when
FactoryTalk Optix Applications
display the tags values.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal