Communication drivers overview
Some communication drivers may have specific characteristics.
IMPORTANT:
For the TwinCAT driver, FactoryTalk Optix cannot import tags of the ITCommObjectServer type because the ITCommObjectServer type is not exported into the TwinCat tpy file.
Communication driver | Online tags import | Offline tags import |
---|---|---|
Modbus Driver | ||
MELSEC FX3U Driver | ![]() | |
S7TCP driver | ![]() | ![]() |
OMRON EtherNet_IP driver | ![]() | |
MELSEC Q driver | ![]() | |
S7 TIA PROFINET driver | ![]() | ![]() |
OMRON Fins Driver | ![]() | |
CODESYS Driver | ![]() | ![]() |
TwinCAT driver | ![]() | ![]() |
Serial port | ||
RA EtherNet_IP Driver | ![]() | ![]() |
Provide Feedback