Configure the grid in the User Interface Editor

Configure the grid in the User Interface Editor

Configure the grid in the User Interface Editor to show or hide the grid, align objects in the grid, and size the grid.
  1. In
    Project view
    , double-click a window or container object, or select
    Editor
    .
    The editor opens in a new tab.
  2. In the editor toolbar, select
    Configure
    .
  3. Select the option to configure the grid:
    • Grid Visible
      . Toggle showing the grid in the editor.
    • Snap to grid
      . Align the edges of objects with the grid.
    • Grid size
      . Specify the size of the grid in pixels.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.