Editor for the user interface
Open the editor for the user interface by opening a window or object.

Item | Description | Icon | Description |
---|---|---|---|
![]() | Tab of the open window or object | ||
![]() | Canvas that displays the open window or object | ||
![]() | Design area for the contents of the open window or object | ||
![]() | Editor toolbar with icons and options that depend on the objects selected in the design area | ![]() | Select . Select items in the design area. |
Rectangle . Draw a rectangle in the design area. | |||
Ellipse . Draw an oval in the design area. | |||
Line . Draw a line in the design area. | |||
![]() | Polyline . Draw a polyline in the design area. | ||
![]() | Send to back . Send the selected object to the back of the objects in the design area. | ||
![]() | Send backward . Send the selected object back one object in the design area. | ||
![]() | Bring forward . Bring the selected object forward one object in the design area. | ||
![]() | Bring to front . Send the selected object to the front of the objects in the design area. | ||
![]() | Left align group . Align the selected objects along the left most object. | ||
![]() | Top align group . Align the selected objects along the highest object. | ||
![]() | Right align group . Align the selected objects along the right most object. | ||
![]() | Bottom align group . Align the selected objects along the lowest object. | ||
![]() | Dock left . Anchor the selected objects on the left while maintaining margins. | ||
![]() | Dock center . Anchor the selected objects vertically while centering the objects and resetting margins. | ||
![]() | Dock right . Anchor the selected objects on the right while maintaining margins. | ||
![]() | Dock left and right . Stretch the selected objects horizontally across the container. | ||
![]() | Dock top . Anchor the selected objects at the top while maintaining margins. | ||
![]() | Dock center . Anchor the selected objects horizontally while centering the objects and resetting margins. | ||
![]() | Dock bottom . Anchor the selected objects at the bottom while maintaining margins. | ||
![]() | Dock top and bottom . Stretch the selected objects vertically across the container. | ||
Delete . Remove the selected object from the design area. | |||
![]() | Select the language for the objects in the design area. | ||
![]() | Select the zoom level for the design area. | ||
![]() | Select options to specify the visibility, snap placement of objects, and size of the grid. |
Provide Feedback