Drawing tools

Drawing tools

Use drawing tools to create custom graphic objects to appear at runtime.
Use the drawing tools to draw free-form and one-dimensional objects including:
  • Rectangles and squares
  • Ovals and circles
  • Lines
  • Polylines and polygons
By default, each drawing object has a
MouseDown
event and
MouseUp
event to which you can add methods that the event performs.
To prevent a drawing from snapping to the grid as you draw, in
Configure
, clear
Snap to grid
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal