- Getting started
- Using the software
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Resize the window
Set the size of the window object to specify the size of the Design Area.
- InProject view, select the window object.
- InProperties, inHeight, enter the value for the height of the window.
- InWidth, enter the value for the width of the window.
- (optional) InFull Screen, selectTrueto make the user interface the same size of as the screen at runtime.
Provide Feedback